Vicor Wins Another ACE Award

December 15, 2016
By

Vicor ACE Award Winner 2016After the success of the Bus Converter Module (BCM) last year, our 48 V Direct to PoL solution was named as the winner in the power category of the ACE (Annual Creativity in Electronics) Awards 2016.

The ACE awards, which are organized in partnership with EE Times and EDN, are very competitive, and considered one of the most prestigious awards in the electronics industry. Vicor, and the other award winners, were announced at the ACE Awards event at the San Jose Convention Center on December 7, during Embedded Systems Conference (ESC) Silicon Valley.

Our 48 V Direct to PoL solution offers significant benefits. It not only replaces a large number of components with just four, but can also be easily scaled to deliver from 50 A to 400 A at voltages from 0.6 V to 2.0 V, for both processor and DDR memory loads.

Check out the Vicor website for more information about our 48 V Direct to PoL solution for datacenters and other computing applications.

Tags: , , , ,

Comments are closed.

Find out more about our Cool-Power Buck Regulators subscribe to vicor newsletter Contact Us

Get Connected