Embedded News Discusses the Benefits of the Power Component Design Methodology with Claudio Tuozzolo

November 29, 2014
By

During the recent electronica trade show, Carolina Kleinken-Palma, editor of Embedded-News.tv, interviewed Claudio Tuozzolo, president of Vicor’s Picor division about the benefits of Vicor’s power component design methodology.

In the video, Claudio explains how the modular and scalable approach enables power system designers to develop high-performance solutions for a wide range of applications. He gives an example of a system that uses a product based on the VIA packaging technology that was unveiled at the show to produce a 48 V hub voltage. This hub voltage can be directly converted to voltages as low as 1 V or less using our PoL regulators.

The interview also discusses a number of other topics, including the importance of efficiency in modern power systems. View the full video below:

 

Tags: , , , ,

Comments are closed.

Find out more about our Cool-Power Buck Regulators subscribe to vicor newsletter Contact Us

Get Connected