Meeting Conducted Noise Standards

March 30, 2012
By

Marco PanizzaFinding an efficient, compact solution to meeting EMI requirements is a greater challenge than ever.

In the USA and Europe, conducted noise emissions are governed by the Class A and Class B limits of both FCC and VDE standards. In the USA, the FCC requires compliance with Class A for equipment operating in factory settings and Class B—the stricter standard—for equipment destined for home use.  In Europe, all countries require that equipment for both home and factory use meet the VDE Class B standard.

The FCC and VDE standards are familiar worldwide and the basis for many local standards. Meeting FCC/VDE Class B limits allows equipment to be operated in most settings anywhere.

“Conducted noise” refers to noise currents on the input power lines which are generated by high frequency switching circuits within equipment connected to the lines. These noise currents, which include common mode and normal mode noise, flow between the power source and the equipment power supply and find their way back onto the power lines. Common mode conducted noise current is the unidirectional (in phase) component in each of the two power lines, which generally finds a return path via the third (earth ground) wire. Normal mode conducted noise current is the component of current which is opposite in direction or phase in the two power lines.

How to Measure

Conducted noise measurements may be made using either a receiver or a spectrum analyzer in conjunction with related equipment to obtain sufficient sensitivity and overload protection to ensure accurate, repeatable measurements of all emissions over the frequency range of 100kHz to 30MHz. Both the equipment under test (EUT) and the receiver or analyzer are connected to the power source through a line impedance stabilization network (LISN).

Setup for measuring conducted noise emissions

The LISN provides power line frequency (50- 60Hz) coupling between the EUT and the power source, while ensuring a high degree of isolation over the spectral measurement range. The receiver or analyzer provides a 50 ohm termination to the LISN measurement port. This guarantees a fixed or calibrated relationship between conducted EMI current and the resulting voltage at the input of the measurement apparatus.

To learn more about how EMI, and how to design in solutions to reduce its impact on the equipment you are designing, watch the rebroadcast of our webinar, “EMI Characterization and Filtering”.

To see the full range of Vicor products, go to vicorpower.com

Tags:

Comments are closed.

Find out more about our Cool-Power Buck Regulators subscribe to vicor newsletter Contact Us

Get Connected